10/20/2023

Delta at the Global OCP Summit 2023: Cutting-edge Server Power Solutions for AI Data Centers


The OCP Global Summit, an annual event for the global cloud and data center industry, wrapped up in San Jose, California, USA in mid-October. Under the theme of ORV3, Delta demonstrated solutions and products such as racks, power supplies, and thermal systems. Among them are the ORV3 power shelves and DC-DC converters, which ensure energy efficiency of the fast-growing AI server segment. These ORV3 power shelves boast 18kW and 33kW power output and up to 97.5% energy conversion efficiency while the cutting-edge DC-DC converters deliver smooth conversion of various power voltages with efficiency as high as 98.3%.

Ares Chen, General Manager of Power and System Business Group, said, "In 2022 alone, Delta’s power solutions for servers and related ICT infrastructure saved over 3.39 billion kWh of electricity for our worldwide customers by leveraging our five-decade core competence in high-efficiency power electronics. The releases of AI chatbots and similar applications accelerate the demands of AI servers while bringing new challenges to server power supply manufacturers. We will continue to focus on ‘higher power output, density and efficiency’ and to collaborate closely with our computing giant customers to ultimately align the megatrends of AI and sustainable development.”

AI learning and training require a foundation of specialized high-level servers. Compared to regular servers that only applies to CPUs, an AI server usually requires four to eight GPUs in addition to two CPUs to perform AI computing and much higher peak power than traditional servers. Delta presented the ORV3 power shelves which feature a 6-slot chassis to accommodate 3kW or 5.5kW power supply units with a maximum power of 18kW or 33kW separately for high-power AI servers. The power shelves could also be designed with 5+1 redundancy to ensure the stable operation of AI servers. Aside from the ORV3 products, Delta also presented the high-power 120kW power shelf which consists of twenty-four 5kW power supply units with up to 97.5% power conversion efficiency. This power shelf can also be configured into a 60kW 2N redundancy power system to ensure high stability and reliability for both AI and traditional servers.

As to DC-DC conversion, the inevitable high-voltage power transmission of AI servers heightens the demands of DC-DC converters between 48V server boards and 12V components. Delta exhibited the RBC and UBC Series DC-DC converters suitable for the applications. Both Series are in compliance with the PMBus communication protocol. The RBC Series features an up to certified 98.3% efficiency, 0.5 – 1% higher than traditional ones. The UBC Series boasts a 5,300 W/inch3 high power density and a bi-directional function to convert from 48V to 12V and vice versa to satisfy various customer needs.

News Source:PSBG_MKT