7/13/2015
Delta completed integrated power solution for the leading fixed-line operator in Poland
Vertical: Infrastructure
Delta MCIS has completed the installation of a 1 Mega Watt UPS system for one of the largest fixed- line operators in Poland. The system supplies a newly-built data center with a target capacity of 800 kW.
As an integrated solutions provider, Delta helped the client develop an electrical and installation layout design and set up an integrated power solution which incorporates Delta's
Ultron DPS 200kVA UPSs, solar inverters, solar panels, and much more. Delta will create a complete PV installation, whose power will be fed to UPS output terminals, limiting grid energy consumption by up to 5%. Such an installation is known as green data center and lays down new trends in the design of UPS systems.