Shoe sole manufacturing starts as the body of the shoe is tightened on the upper mold and the station is heated at the same time. The molten foam rubber is then cast and poured into the lower mold. As the two molds close, the materials begin foaming and expanding. After cooling and forming, the process of shoe manufacturing is complete.

Delta’s Cartesian Casting Robot Solution adopts Delta’s Robot Controller with its Servo Drive Integrated ASDA-MS Series, integrating robot controller and servo drive in a single unit. The ASDA-MS Series connects with the Compact Modular Mid-range PLC AS Series through the Delta Motion Control Network DMCNET to control other equipment such as mold closing and foaming at a far distance.

The ASDA-MS Series collaborates with the Human Machine Interface DOP-100 Series and Widescreen Handheld HMI DOP-H07 Series. The HMI DOP-100 Series offers real-time status of the system and supports mixed-model production. In terms of the handheld HMI DOP-H07 Series, the built-in teach pendant function enables robot operating points and path type recording, achieving high speed, precise positioning, and smooth movement.