9/15/2011
2011 Serial Communication Solutions from Delta Electronics
Differences in communication protocols used by various industrial automation products makes it costly to integrate products from different manufacturers. To meet this need, Delta Electronics offers the DVPSCM12-SL communication module as a complete solution to serial communication.
The DVPSCM12-SL hardware has two sets of built-in RS-485/422 serial communication interfaces that separate communication and power to effectively enhance the product's capability to resist interference and overcome all sorts of adverse application environments. There are built-in 120Ω terminators and drop-out screwless terminal blocks that save time and cost for wiring. In addition to the built-in Modbus communication protocol, the most frequently used in industry, the DVPSCM12-SL also features a programming software for open-platform communication protocols, enabling customers to set up various serial communication protocols in a speedy manner. The DVPSCM12-SL can be expanded to function as a communication port (COM3) of the PLC host for up- and downloading PLC programs and monitoring PLC parameters, and it reduces loads for PLC host communication. The DVPSCM12-SL is suitable for building and factory automation. It lets system manufacturers overcome difficulties in connecting different communication protocols.
For more information, please go to:
Delta Electronics
Delta Industrial Automation Products