6/15/2009

Tip of Delta HMI (1) : Screen Data Convert

Q: How to quickly convert the HMI project of DOP-A series to DOP-B series?


A: Screen Editor 2.00 configuration software provides screen data convert function. Just in three easy steps and the users could covert the HMI project of DOP-A series to DOP-B series quickly.

1.Enable Screen Editor 2.00.08 software. Select the File Menu – Open or use the keyboard shortcut Ctrl + O to open an old project. When Open dialog box appears, select a dop file from this dialog box, and click the Open button.


2.Select a DOP-B series model, and click the OK button.


3.Execute Compile function, and then the project can be downloaded to DOP-B series HMI.

Please note: As the resolution and proportion of DOP-A series and DOP-B series are not the same, after the HMI project is converted, it still needs to adjust the element position and text size, etc. settings manually for the best display effect.

News Source:Delta IABU PSM