Step 1: Connect to the drive via VFD Explorer Lite as follows:
Image 1. VFD Explorer Lite connection steps
Step 2: After connecting, click PR to open the control screen → click Load Pr. to read the parameters of the drive.
Image 2. Read the internal parameters of the drive
Step 3: Select the drop-down menu parameter 09 Communication → Fill in the IP address and subnet mask of parameters 09-76~09-83. If the parameter number already has a value, make sure to re-enter it.
Image 3. Select the communication parameter group and enter the IP and mask value of the corresponding parameter
Step 4: Set parameter 09-91 as 2 and write the IP into the communication card.
Image 4. Write the IP and subnet mask settings into the communication card
Step 5: Use Load Pr. to re-read the parameters of the drive and check whether parameter 09-91 is reset to the default value of 0. If it is reset to the default value, then the IP address is successfully written.
Image 5. Check whether parameter 09-91 is reset to its default value