Is there encryption for Delta’s CNC controller Macro program?
Yes, please refer to the instructions below.
1. Turn on “O macro file protection” in parameter 10016 and then restart.
2. You will see the “O_MACRO_ECP” folder automatically generated under INTER. Move the MACRO files to the folders for encryption. (Naming rule: O9000 ~ O9999). The system will automatically encrypt the files and save as “.CPRS” files.
3. After encryption, the system will search the folder “INTER:\O_MACRO_ECP\” while calling the MACRO program and executing the encryption files.