How do I add more AS Series PLC data exchange tables?
Q: In the AS200/AS300, the maximum number of data exchange tables is 16/32, while users often ask for more. How do I add data exchange tables?
A: Modify the parameter via the CCONF Command to add data exchange tables. Please refer to the example below: