How do I set TCP Socket and confirm whether the connection is successful with the Compact Modular Mid-range PLC AS Series?
1. Connection configuration setting: Use a PC as the server and the AS Series as the client to set a TCP connection.
2. ISPSoft→HWCONFIG settings:
3. Build connection: Check whether the Socket you want to connect is off (SM1274=On), not connected (SM1270=Off) or not in connection building (SM1273=Off) when M0=On. If the condition is true, the connection will start to process.
4. Determine if the connection is successful
A. Check the connection status (SM1270=On)
B. Use CMD and input
netstat –na to confirm whether the TCP connection status is Established.