If the users want to change their HMI from 5.7 inches to 10.4 inches models, do they need to rewrite the program files? If not necessary, how to solve the problem that if the resolution is different?

The users do not need to rewrite the program files as the screen editor software will automatically adjust the elements in a ratio of equality. It means that the elements in 320 x 240 pixels stored in 5.7 inches model could be adjusted to the elements in 640×48 pixels stored in 10.4 inches model.