How do I calculate the optical resolution when using the DMV3000 Series to detect objects?
The flow chart of Fig. 1 shows the process.
1. Refer to page 17 in the DMV3000 User Manual (Fig. 2).
2. Define a camera FOV range.
3. Select a camera and a lens.
4. Find an online lens calculator to calculate the optical resolution.
If the resolution does not meet your requirements, go back to Step 3 and reselect a camera and lens.
Fig. 1: Flow Chart

Fig. 2: Page 17 in the DMV3000G User Manual