How do I use the ComboBox function in the DIAView SCADA System?
1.Click ComboBox in Toolbox, and then click and drag on the right pane to create a new ComboBox.

2.Add sub-groups to the new ComboBox.

3.Select the new ComboBox0.SelectedIndex and click SelectionChanged under Event to trigger and run a function (A, B, or C function).

4.Click different sub-groups under the new ComboBox to switch pages or functions.