How do I use CNCSoft to transfer machining program files from the computer to the CNC controller?

Use CNCNetwork in CNCSoft to transfer machining program files from the computer to the CNC controller.


1.Start CNCNetwork, click “Setting” and set the Local Area Network (The controller and the computer have to be in the same LAN). Click “Search CNC” after setting.


2.The controller name and IP appear in the bottom left column. The disk space is shown in the right column in “Management”



3.Select the file folder to upload and download the files.