What are the features of the PR mode function in AC servo drives? Which of Delta's AC servo drives supports this function?

With the PR mode function, the profile command is generated in the servo drive, and the host controller only performs sequential control. Currently, Delta’s AC Servo Drive ASDA-A2 and ASDA-A3 Series support the PR mode function. The ASDA-A2 Series provides 63 profiles, and the ASDA-A3 provides 100 profiles, including homing mode, position command, speed command, jump command, write command, index positioning command and basic numerical operation.