How does an end user download Delta PLC programs without opening a project file in the editing software?
Convert the project file into a DVZ file with the Delta EasyDownload program, and ask the end user to download the file. Please refer to the steps below:
1.Create a DVZ file.

i. Open the Delta EasyDownload program, and choose “Create DVZ file”
ii. Select a WPL or ISP project file to download, and download parameters if needed.
iii. Select the file path to save and finish creating the DVZ file.

2.Download the DVZ file to Delta’s PLC (for the end user):
i.Open the Delta EasyDownload program, and choose “Write DVZ file to PLC”

ii.Select the DVZ file to download.

iii.Select the PLC communication method to connect and the DVZ file will download to the PLC.