How do users set up time intervals and saving intervals when using the Multifunctional Power Meter’s programming software DPMSoft?

When using the Multifunctional Power Meter’s programming software DPMSoft to set up Delta’s Multifunctional Power Meter DPM Series, users can find two major sections on the saving record page: one is time interval and the other is saving interval.

1. Saving interval setup: Based on different requirements, users can set up parameters to be saved under this column, such as voltage, current, and more. Different saving intervals reflect different quantities of saved parameters, which are specified below:




2. Time interval setup: Users can define how long the power meters sample the measured data. After setup, the power meters sample and save the selected parameters based on the set up time interval, to record measuring data.