What other communication interfaces do Delta AC motor drives support besides the standard MODBUS protocols?

Delta's new generation AC motor drives C2000 series, CP2000 series and C200 series also support PROFIBUS-DP, Device Net, MODBUS TCP and EtherNet/IP cards and these high speed communication interfaces are all available as optional accessories. The C2000 series and VFD-VL series also offer a built-in CANopen protocol and the CP2000 series offers a built-in BACnet communication interface.