How will the motor’s torque be when V and f are changed in proportion?
The voltage will be reduced with frequency in proportion. The torque is also decreased in low speed because the reduced AC resistance and the constant DC resistance. Therefore, it can get higher start torque by increasing output voltage in the low frequency. Many methods can be used to get it, such as auto torque compensation, high start torque V/f curve and potentiometer adjustment.