Healthy Lighting

As technology continues to advance at an unprecedented pace, an increasing amount of research has revealed the significant impact of lighting on health. Taking circadian lighting as an example, Delta's intelligent lighting system can emulate the natural variations in light, aiding users in maintaining a balanced biological clock, improving sleep quality, and regulating mood. Delta has taken it a step further by introducing products that target different wavelengths and frequencies of light, including 222nm safe UV disinfection and 40Hz brain-care products. Leveraging exceptional in-house research capabilities and a robust engineering team, Delta has centered its development on various health-oriented lighting products with "light" as the core focus. Delta's aspiration is to continually innovate in health applications, deepen the understanding of light's influence on the human body, and create more possibilities for the future.