2/24/2017
Delta Articulated Robot Wins Silver Award at the 25th Taiwan Excellence Awards
The winners of the 25th Taiwan Excellence Awards and its Gold / Silver Awards were just unveiled, and Delta's Articulated Robot DRV70L / DRV90L has won the Silver Award. Five other Delta automation products were also awarded Taiwan Excellence Awards. Delta's awards included the:
• Delta Articulated Robot DRV70L / DRV90L Series – Silver Award
• IP55 Fan & Pump Drive CFP2000 Series – Taiwan Excellence Award
• Standard / High Performance Compact Drive MS300 / MH300 Series – Taiwan Excellence Award
• Compact Modular Mid-range Controller AS300 Series – Taiwan Excellence Award
• High Performance Servo System ASDA-A3 Series – Taiwan Excellence Award
• Machine Vision System DMV2000 Series - Taiwan Excellence Award
All six of the award-winning products were newly launched in 2016. Among these, the Articulated Robot DRV70L / DRV90L Series, launched in September, 2016, was a stand out for winning the “Silver Award” for its elegant, eye-catching appearance and multi-angle processing capability. The DRV70L / DRV90L Series are suitable for complex processes such as insertion, screw locking, assembly, coating, transfer, soldering, transporting, and packaging for the consumer electronics, electrical/electronics, rubber and plastic, packaging, metal fabrication and other industries.
The DRV70L Series has completed SCARA robot function tests in Delta's Wujiang Plant, which allows operators to complete five function tests with one simple click. The implementation of the DRV70L Series successfully reduces manpower, shortens testing time (from 68 min. to 18 min.) and enhances testing efficiency by 74%. In addition, this articulated workstation is connected to the Manufacturing Execution System (MES) to provide full production traceability and enhance productivity and product quality.
With six industrial automation products winning Taiwan Excellence Awards, Delta has proven to be one of Asia's leading automation products and solution providers. Delta continues to practice its brand promise “Smarter. Greener. Together.” as it develops more innovative automation products and solutions for future industry and smart manufacturing.
Delta's industrial automation products that have won Taiwan Excellence Awards, include:
• IP55 Fan & Pump Drive CFP2000 Series, which features highly effective protection against dust and water in harsh environments, and is perfect for fan and pump applications. The CFP2000 Series has a built-in EMC filter and DC reactor and provides high integration for enhanced efficiency. It supports induction motor and permanent magnet motors, built-in STO (Safe Torque Off) function, PLC programming (10k steps) and a variety of industrial communication protocols. With parameter pre-setting and a multi-language interface, the CFP2000 Series offers a simplified adjustment process and a user-friendly interface for flexible applications.
• Standard / High Performance Compact Drive MS300 / MH300 Series are Delta's new high frequency, high power compact drives. With up to 40% size reduction, the MH300 / MS300 Series are the smallest AC motor drives Delta has ever offered. They save installation space and provide user-friendly installation and operation for customers.
• Compact Modular Mid-range Controller AS300 Series is Delta's new advanced modular controller for automation machinery. With new 32 bit SoC (System on Chip) CPUs, the AS Series offers excellent performance with a program capacity of 40k steps/ms and supports up to 32 extension modules or a max. 1,024 I/O points. It is able to control max. 8 axes via CANopen motion network / max. 6 axes via pulse control (200kHz).
• High Performance Servo System ASDA-A3 Series is designed for advanced machines and motion systems. It offers advanced built-in motion functions for PLC-based and PC-based motion control systems to fulfill industry needs. Delta's ASDA-A3 Series features new flexible algorithms and motion compensation to easily eliminate vibration and enhance production efficiency. The new auto-tuning provides simple setup and shortens adjustment time for customers. The size of the ASDA-A3 series is compact and light and it is 20% smaller than Delta's ASDA-A2 series for efficient space savings. In addition, with 3kHz high frequency response and 24-bit high resolution absolute type encoder equipped as standard, the ASDA-A3 series is ideal for CNC control systems to provide better synchronous motion commands, smooth operation at low speeds, and superior surface finishing.
• Machine Vision System DMV2000 Series supports synchronous multi-camera vision inspection. It features high speed and stable image capture and transmission, and ensures product quality and automation production efficiency. It provides a smart operation process and interface and multi-function modules to shorten system development time and enhance customer satisfaction.