1/21/2014
Delta Unveils Energy-Saving and High-Performance Servo Drive Solutions at Plastivision India 2013
A prosperous manufacturing sector has contributed to India's steady economic growth and has stimulated the growth of the plastic products market. The demand for plastics processing and manufacturing equipment has also increased in its wake. One of the biggest marketplaces for plastics manufacturers, the 9th Plastivision India 2013 was just held in Mumbai from Dec. 12 through 16 of 2013. Delta was on hand to showcase a full range of automation solutions and products with features on servo drive solutions that are energy-efficient, high-performance, and suitable for plastics manufacturing applications.
During the five-day show, Delta put the spotlight on its energy-efficient Hybrid Energy Saving System (HES). The HES, when applied to plastics injection molding, can achieve up to 40% to 60% of energy savings compared with using traditional variable or quantitiative pump hydraulic systems. It also uses an oil temperature that is lower by 5~10°C, with advantages for 50%~60% oil savings, as well as space savings for oil tanks, and a lower requirement for coolers used during processing.
Another attraction at the Delta booth was the multi-axis high-speed synchronous servo drive solution. The integration of Delta's servo drive ASDA A2-E Series with Delta's HMI supports the EtherCAT communication interface for exceptional operation speed and performance. This is particularly ideal for engraving machines and many other plastics processing applications.
Organized by the All India Plastics Manufacturers' Association, Plastivision has been held once every three years since it's first launch in 1986. This year's show attracted more than 1,000 manufacturers of plastic materials and processing equipment, as well as 70,000 visitors. Plastivision has emerged as India's most prestigious event for the plastics industry and is shaping up as one of the world's top 10 plastics shows.
The line of Delta Industrial Automation's solutions and products brought more than 150 guests to our the booth. With the brand promise "Smarter. Greener. Together.", Delta continues its dedication to providing innovative, clean and energy-efficient solutions for a better tomorrow.