9/11/2020
Delta Controls Launches enteliCLOUD for Cloud-Based BMS
Delta Controls is currently in the process of launching an exciting new product: the enteliCLOUD, a cloud-based BMS service.
The enteliCLOUD is a cloud service that securely acquires, transfers, and stores building automation system data to improve organization, management and savings. With enteliCLOUD, our customers can monitor, operate and control their portfolio buildings across geographies with a computer or smart device.
There are notable differences between the enteliCLOUD and our enteliWEB product, but in all other regards, the same features and functionalities exist between the two products. The enteliCLOUD is a more user-friendly version of enteliWEB. It has many features that are automatically built-in and set up, such as deployment, HTTPS/SSL Installation and Public DNS. With enteliCLOUD, users can subscribe monthly to the licensing and can manage their site from the portal. With enteliWEB, the above features are user-managed and configured.
The enteliCLOUD has many impressive features such as Remote Access Control, which allows users to monitor and control their buildings from home, the office or on the go without requiring onsite staff. This feature allows for significant cost-savings since a building manager does not have to pay for full-time staff onsite. Another great feature is the Renewable Energy Management that the enteliCLOUD offers. This feature manages renewable energy sources in conjunction with energy consumption. It is not only beneficial when it comes to saving money, but also when making a positive impact on the environment.
Another great feature this product has is it allows users to Optimize their Business Tactics. The enteliCLOUD keeps up-to-date building performance data, allowing users to make better business decisions along the way.
We are very proud of the enteliCLOUD and know that it will be another key product of ours. Not only does it allow companies to manage their buildings in more efficient ways, it truly does help reduce costs. There is no need for costly emergency technician visits because the enteliCLOUD allows building managers to pre-diagnose problems and fix them remotely from wherever they are.
enteliCLOUD is the future of operational excellence. It delivers a consistently exceptional employee and customer environment and also helps boost staff productivity. Delta Controls is delighted to be behind another ground-breaking product and cannot wait to help businesses increase the value of their portfolios with enteliCLOUD.
Learn more about enteliCLOUD product information.