11/5/2015
Delta Electronics' Vivitek Qumi Q6 LED Mobile Projector Wins 2015 Good Design Award
Taipei, Taiwan, Nov. 5th, 2015 - Delta Electronics, a leading global company in smart green solutions, has just received the Good Design Award for its Vivitek brand Qumi Q6 LED mobile projector at an award ceremony held in Tokyo midtown on Nov. 4th. Mr. C.H. Ko, executive director of Delta Electronics (Japan), attended the Good Design Award ceremony on behalf of Delta as the company was recognized for its high-level product design.
“Qumi Q6 is well equipped with all the functions necessary for a projector in such a compact design,” commented a judge for the Good Design Award. “When the Qumi Q6's built-in wireless functionality connects with a smartphone, tablet, or PC, it enhances personal applications in addition to conventional business applications.”
The Qumi Q6 is a mobile projector featuring an extremely light weight of 475 grams with a high brightness of up to 800 lumens and a 30,000 contrast ratio. Despite its compactness, the Q6 can handle projection up to 50 inches in a bright environment, 70 inches in a dim environment, and 90 inches in a dark environment. Users can easily carry the Q6 around in a briefcase and enjoy its large screen projection at business meetings while a conventional projector requires space and fixtures. The Q6 is also equipped with an LED of over 30,000 hours long life as a light source, allowing users to reduce operating cost since exchanging the lamp is not necessary.
The annual Good Design Award started in 1957. It is hosted by the Japan Institute for Design Promotion, a public interest incorporated foundation, and is the only award in Japan to comprehensively evaluate the design and functionality of various products every year. Submissions come from a wide range of fields, and roughly 1200 designs are recognized every year. Over 59 years, around 42,000 designs have been recognized by the awards. Recipients of the Good Design Award are granted use of the G Mark symbol, which has been an emblem of good design for over half a century.
Since the Qumi projector series was first launched in 2011 it has won many design awards from professional media around the world with its stylish appearance and rich interfaces. These awards include the British "AV Awards 2011 Finalist ", the Americas "PRODUTO DO ANO EDITOR" annual Editor's Choice, as well as China's "PC HOME" Best Creative New Product Award and Best Design Award. The Qumi Q6 also won Taiwan's Golden Pin Design Award in September and Japan's Good Design Award at the end of this year.