2/10/2015
Delta demonstrates its leadership in Display Solutions with the world's first Laser-based (DLP®) Video Wall at ISE 2015, Amsterdam
Amsterdam, The Netherlands, February 10, 2015 - Delta Electronics, Inc., a global leader in power and thermal management solutions and pioneer in display solutions, announced today it will unveil, at Integrated Systems Europe (ISE) 2015, the world's first ultra-bright Laser-based Digital Light Processing (DLP®) video wall which features industry-leading performance with brightness of up to 1,800 lumens and significantly improved energy savings of up to 10%. Visitors will experience a live demonstration of Delta's advanced vision control systems –DVCS(1) and MiNiCON(2)– which turn our innovative video walls into comprehensive display and monitoring solutions for applications demanding 24/7 operations.
Delta will also showcase its revolutionary Industry Intelligent Monitoring Management System, iPEMS™(3) at ISE 2015. The highly adaptable and customizable iPEMS™ is a living proof of Delta's profile as a total solutions provider since it integrates IoT technology with Delta's DVCS advanced vision control system. iPEMS™ enables monitoring of more than 10 million supervision points in real-time, ultra high-resolution visualization with intuitive SCADA graphics and with big data mining and analysis capabilities. These features have, for example, become a valuable support for effective decision-making processes within the industrial operations of a major oil & gas firm, thus, helping realize significant improvements in both operational and energy efficiency.
Delta's capabilities in integration of advanced software and hardware display technologies will be palpable at ISE 2015 through the showcase of our highly adaptable and expandable IP-based DVCS and the fully embedded MiNiCON vision control systems which combined with our video walls represent a total display solution for mission-critical, control-room and broadcasting applications.
The Ultra Slim Cube Series video wall features WUXGA (Wide Ultra XGA, 1920x1200) resolution, super-efficient LED light engines, auto alignment, and auto color calibration. The hot swappable power supplies of the Ultra Slim Cube Series ensure high transfer efficiency and reduce power consumption by more than 10% as compared to standard cubes. In addition, Delta will offer a sneak preview of its ultra-narrow bezel LED LCD video walls, featuring the slimmest bezel in the market. These video walls allow a seamless connection between each display to create a powerful, high-impact visual experience for viewers.
For business and education applications, Delta's WX displays will demonstrate how multiple users can access and share content on a super-large digital canvas simultaneously by using their own mobile devices over an existing WiFi or Ethernet network. Bright, high-impact 1.8mm and 4mm indoor LED displays and LCD Monitors showcased at the front of Delta's booth, deliver visual excitement to indoor environments. Delta will exhibit the aforementioned display & monitoring solutions during ISE 2015 at booth 9-F111, Amsterdam RAI, from February 10th to 12th, 2015.
Notes:
(1) DVCS: Distributive Vision Control System.
(2) MiNiCON: Embedded Vision Control System.
(3) iPEMS: Intelligent Monitoring & Management System.