Taipei, March 5, 2015 – Delta Industrial Automation, the leading global provider of integrated CNC and machine tool system solutions in Taiwan and China, is showcasing its latest technologies and solutions including its high-end CNC system solutions and new SCARA Robot at the TIMTOS 2015 exhibition (Taipei World Trade Center, Hall 1#B0418) from March 3 to 8.
With its business motto “Automation for a Changing World”, Delta IABG is dedicated to developing and providing innovative, high performance and high quality automation products to fulfill a wide range of industrial customer needs around the world. Delta IABG General Manager, Mr. Simon Chang, said, “The machine tool markets of Taiwan and China rank 7th and 1st in the world respectively. To provide more flexible and cost-effective solutions to the market, Delta has introduced customized CNC system solutions to benefit our customers.” As one of the first Taiwanese companies to offer CNC solutions, Delta also provides a complete range of products for the machine tool industries, including CNC controllers, multi-axis servo drives and motors, and PM spindle servo drives and motors. Delta's CNC solutions are also currently succeeding in European markets such as Germany and Italy, enhancing machine tool efficiency and precision for global customers.
At TIMTOS 2015, Delta is showcasing a total of 10 high-end integrated machine tool solutions, including a high speed tapping machine, dental milling machine, vertical machine center, as well as tool turrets solutions. Delta is also demonstrating its intelligent robotic arm solution including the SCARA Robot and 5-axis Cartesian coordinate robotic arm system.
Product highlights include:
CNC System Solutions
- High Speech Tapping Machine (Solution from Delta; Machine from Fair Friend Group)
This solution adopts Delta's CNC controller, multi-axis servo drives and spindle motor to perform high precision and synchronized rigid tapping with 6,000rpm to 12,000rpm in 355ms (0.335 second). Under the rated speed of 6,000rpm, the tapping machine delivers high speed performance with 0.88 second per tapping. In addition, the system offers power regeneration, and is able to transform the energy generated during instant braking into reusable power with a Delta C-Box, saving up to 70% energy.
- Dental Milling Machine (Solution from Delta; Machine from DMARK)
Delta's CNC controller and distributed motion control system for this dental milling machine performs with an excellent 8KHz response speed. Delta servo drives also provide a fine interpolation function for a smooth speed and greatly enhanced surface finish. The dental milling machine features high speed, high precision, and superior surface finishing and stability.
- Vertical Machining Center (Solution from Delta; Machine from Yang Iron Precision Corp.)
Delta's integrated CNC solution delivers excellent performance for this vertical machining center with a CNC controller, servo system, PM spindle motor, and machine vision system. It is capable of performing tasks requiring high precision, high quality, efficiency, a short processing time, and fine surface finishing, such as milling, boring, drilling, screw thread tapping, screw cutting and many other complicated machining processes. The vertical machining centers are used to manufacture many types of components in industries such as machinery, automobiles, architecture, injection molding, and many more.
- Turret and Automatic Tool Changer (ATC) Solutions
Delta's turret and ATC solutions feature high tool changing efficiency, high system stability, and are also anti-noise, impact resistant, and oil resistant. Delta's Turret and ATC solutions are now available in the markets of Germany and Italy, bringing high efficiency and benefits to customers.
SCARA Robot Solutions
Delta's new SCARA Robot DRS40L Series and industrial robot solution features high-speed, high precision, and compliance control functions. It has been successfully applied in Delta's Wujiang and Taoyuan plants with the benefits of tripling productivity and significantly lowering manpower costs.