Please enter your profile and select news type(s) you want to subscribe to. We’ll start delivering Delta news via email alert after your account being activated.
 
Press Releases
  2017/05/31  
  “Delta Physical World” Showcases Delta’s Integrated Solutions and Latest Consumer Applications at COMPUTEX 2017
 
   
   
Taipei, Taiwan, May 31, 2017 – Delta, a global leader in power and thermal management solutions, is exhibiting at COMPUTEX TAIPEI 2017 from May 30 to June 3, its latest interactive systems, energy management platforms and advanced projection, along with consumer brands Innergie and Vivitek for power devices and projection, respectively. Innergie is unveiling its newly-launched PowerJoy 30C USB-C Wall Charger, featuring 5.4A large output with USB-A/USB-C dual ports, while Vivitek exhibits its newest 4K home theater projector HK2288 and ultra-short-throw laser projector DH768Z-UST. Delta’s showcase is under the theme “Delta Physical World”, echoing an interactive technology educational exhibition presented by the Delta Electronics Foundation and the National Museum of Natural Science earlier this year, as physics is essential to product innovation.

Delta’s Chief Executive Officer, Mr. Ping Cheng, said, “In an age in which digitalization is transforming global industries, Delta continues to enhance its innovation capabilities not only in hardware systems but also in management software. By utilizing sensing control and communication technology, Delta is able to integrate hardware and software to offer solutions such as EV charging, building automation, and displays, which are all showcased at COMPUTEX TAIPEI 2017. We also continue to pursue innovation in providing smart solutions in key areas such as smart manufacturing.”

Delta’s Chief Brand Officer, Ms. Shan-Shan Guo, remarked, “We partnered with the National Museum of Natural Science to host the ‘Physical World’ educational exhibition inaugurated in February. It is designed with Delta’s interactive technologies including robotic arms, display solutions and other education applications to inspire the public on the fun aspects of science learning. At COMPUTEX TAIPEI 2017, we use the ‘Delta Physical World’ as the exhibition theme to let visitors experience the Delta’s latest innovative solutions as well as the consumer electronics products of our brands Innergie and Vivitek.”

Visitors at Delta’s booth will experience Delta’s growing capabilities in regards to software and hardware integration: AC and DC EV charging solutions with site management systems enable remote supervision; building automation solutions integrate building sub-systems and execute management and data analysis of entire buildings. Tech-savvy consumers will have access to Innergie’s complete consumer power product lines with the highest safety standards and the brand new PowerJoy 30C USB-C Wall Charger, capable of up to 35% faster charging than original manufacturer chargers and supporting both USB-C and USB-A power outlets. Visitors will be also able to experience Vivitek’s new projectors, the HK2288 4K home theater projector and the DH768Z-UST ultra-short-throw laser projector.

You are welcome to visit “Delta Physical World” at L0818, 4F - Taipei Nankang Exhibition Center during COMPUTEX 2017 from May 30 to June 3.

Highlights of Delta's booth this year are:

Energy Management Area
Building Automation: Delta’s Building Management and Control System (BMCS) incorporates international standard protocols to enable integration of all building operation systems on a single IP-based management platform that offers ease of maintenance and energy savings. Delta Energy Online is an enterprise-grade energy management system with data acquisition, analytics and diagnosis for building energy visualization, auditing, and verification of energy savings achieved.

EV Charging: Delta’s DC Wallbox EV Charger achieves remarkable efficiency of 94%, and its wall-box design and pluggable power module design facilitate higher productivity in regards to installation costs and time. The Delta AC Mini EVSE (Electric Vehicle Supply Equipment) is a compact and stylish device compliant with global charging standards. Delta’s EV Charging Solutions add significant value through the Site Management System which enables highly effective remote setup, management, and maintenance for single and multiple sites.

Datacenter Infrastructure: InfraSuite Manager is a Data Center Infrastructure Management (DCIM) system, integrating all facility and IT equipment onto one platform simultaneously. The EnviroProbe and EnviroStation work together seamlessly to immediately perform the complete management of energy, power system, cooling, environment, security, asset, server monitoring and more, making it an eternally alert sentry to guard your datacenter.

Multimedia Theater and Interactive Area
Vivitek HK2288 Projector: The Vivitek HK2288 4K Ultra HD projector features a 3,840 x 2,160 resolution, and 50,000:1 contrast ratio. The powerful HK2288 is engineered with an energy efficient lamp that lasts up to 4,000 hours (Dynamic Eco Mode). Through vivid color, rich blacks and crisp resolution, friends and family will be instantly captivated by what’s being projected.

Vivitek DH768Z-UST Short-throw Projector: For educational settings, Delta is introducing its first Ultra Short-Throw (UST) Laser projector, the DH768Z-UST. The UST technology ensures that there is no glare in the presenter's eyes and that the image is shadow-free. The DH768Z-UST features full 3D functionality, a 1080p (1,920x1,080) resolution, 4,500 ANSI lumens, 12,000:1 contrast ratio, long life light source for up to 20,000 hours, and is capable of projecting an image of up to 150" (diagonal).

Innergie Consumer Power Products
PowerJoy 30C USB-C Wall Charger: The PowerJoy 30C has one USB-A port and one USB-C port with a large output of 5.4A which enables up to 35% faster charging than original manufacturer chargers. It also includes interchangeable AC plugs compatible with the power standards of more than 150 countries. Visitors can also access the complete Innergie product line including PowerGear ICE 65 universial laptop adaptor, LifeHub Plus super-speed charging hub, and PocketCell power bank.

Ventilation Fans
Luxury300 Heater & Ventilation Fan: The Luxury300 was recognized by Taiwan Excellence 2017. It adopts Delta’s highly efficient brushless DC motor technology and can achieve 50% energy savings compared to traditional ventilation fans. The Luxury300 has comprehensive ventilation functions including heating, cooling, drying, and exhaust function with timer. It also has an LED light with sensors.

Signature series: This series is remarkably energy-efficient with a DC motor. The design offers solid, elegant ventilation solutions with motion and humidity-sensing, and speed options with built-in controls. The series has obtained an ENERGY STAR certificate.

Physical World Area
“Physical World” is an interactive technology educational exhibition organized by the Delta Electronics Foundation and the National Museum of Natural Science earlier this year. The permanent exhibition in National Museum of Natural Science adopts many of Delta’s technologies in power electronics, automation and optics. At Delta’s booth during COMPUTEX 2017, visitors can experience the Newton's Cradle and vertical pendulum wave demonstrations that are popular in “Physical World”.
Delta showcases its integrated capability at COMPUTEX 2017. Delta’s Chief Executive Officer Mr. Ping Cheng (left) and Chief Brand Officer Ms. Shan-Shan Guo introduce Delta’s EV charging solution to media.
News Source: Delta Electronics
     
   
 
  Delta Provides Fast DC EV Charging Solution to Singaporean L...