3/26/2007
Delta@@s High Efficiency Converter Win 2006 Technology Awarded of ECN Magazine
Taipei, Taiwan, March 26, 2007 – Delta Electronics (TSE: 2308), – a worldwide leader in power management products, today announced that it's high efficiency and high power converter selected a Top Winner in the Power Sources Segment by ECN (Electronic Component News) Magazine for their 2006 Technology Awards. Delta's Delphi F48SA280, full brick, DC/DC converter is praised and admired by its' 91.5% efficiency and its max power to 700W.
Specification highlights of the F48SA280 include its typical efficiency of 91.5% at full load and its ability to deliver up to 700W in an Industry Standard full brick footprint and pin-out.
Delta's Delphi Series of Standard Board Mounted Power products covers the gambit of Industry Standard platforms, including full bricks, half bricks, single and dual output quarter bricks, low and high powered eighth bricks, sixteenth bricks, 1x1 and 2x1 products, as well as host of DOSA compliant Point-of-Load products and bus converters.
These results, as well as other winners, may be seen in the December 15th, 2006 issue of ECN Magazine. For more information about Delta's Delphi Series of Standard Board Mounted DC/DC Power Converters, please visit: http://www.delta.com.tw/dcdc/. For further information on this press release, please contact Renee Catalano at 978-656-3993 x 106 or at rcatalano@delta-corp.com.