1/17/2012
Delta Electronics Launches New Series of Air-to-Air Heat Exchanger Cooling Solution for Outdoor Cabinet Applications
Taipei, Taiwan, January 17, 2012 — Delta Electronics, Inc., a world-leading fan and thermal management solutions provider, has launched its the world's first Air-to-Air Heat Exchanger series , capacity from 50W/K to 260W/K, that offers simple and integrated thermal solition to the outdoor cabinet in telecom application. With Delta's advanced thermal design, this optimized solution provides customers with up to 30% increase of energy efficiency to reduce operation cost, in a size that is 50% smaller than traditional heat exchangers. Customer benefits not only from the lower operation cost, but also the saved space that gives its engineers flexibility when system upgrade is needed.
"This is another successful solution of system integration made possible by synergy of Delta's thermal expertise and telecom power cabinet design capabilities, and it fulfills Delta's mission as well", says Wilson Huang, General Manager of Fans & Thermal Management Business Group. The high efficiency thermal solution comes from integration of Delta's patented "Pentagonal Thermal Cooling Core " and optimized fans that significantly increases heat dissipation with less power.
Delta's Air-to-Air Heat Exchanger is designed and tested air tight that provides complete isolation protection for the systems from air contamination, dust, and humidity often seen in outdoor environment. Delta uses highly automated manufacturing process in its production that yields high quality products while maintaining low wastes and keeping its cost competitive. The heat exchanger is designed in compliance with IP55, TUV, CE, and UL, and has passed severe salt fog cycle tests.