News Center Press Releases
Home
News Center
Press Releases
The Other Latest News…
Delta Electronics, Inc. Accomplishes Conditions of Conditional Volunta...
Delta Electronics’ Consolidated Sales Revenues for January 2019 Totale...
Delta Showcases IoT-Enabled Smart Energy-Saving Solutions for Building...
Delta Electronics’ Consolidated Sales Revenues for December 2018 Total...
2014/06/30
Delta Electronics introduces innovative Battery Energy Storage Solution
Delta designed this BESS system for smart grid applications
Label
Label
Versailles, June 29, 2014 - Delta Electronics (TWSE: 2308), a global leader in power and thermal management solutions headquartered in Taiwan, announced today the launch of a new Battery Energy Storage Solution (BESS), at a press conference in Paris. This innovative energy-saving solution is complementary with renewable energy production systems in smart grids, and helps managing energy demand to ultimately reduce or defer the overall costs of grid investment and power dispatch. Delta developed this innovative energy storage system designed for smart grid applications to optimize home energy balance. The system serves as an ‘energy reservoir' for electricity generated from the photovoltaic (PV) module. The electricity which is stored in the batteries in the system can either be used by the household when there is no sunlight, or be fed into the grid when there is surplus energy. Jackie Chang, President and General Manager of Delta EMEA, declared: "thanks to Delta's Battery Energy Storage Solution, the system showed a significant reduction of grid power purchase. This new flexible and modular system helps managing energy in a grid including intermittent energy sources, such as solar energy. With this new solution, Delta contributes to smarter and greener energy management". The Delta energy storage and management system is designed to be modular and flexible in configuration. It can optimize energy consumption and power dispatch according to customer profiles. Significant benefits resulted from the Delta energy storage system include 1. Reducing gird peak power demand; 2. Increasing the utilization of renewable energy, such as the existing rooftop PV installation; and 3. Reducing electricity bills by load shift and avoiding high electricity tariffs. The BESS system is a home energy system consisting of a complete Delta composition, including rectifier, charger, micro-inverter, Li-ion battery, controller, sensor module and an energy management system, which can be remotely-controlled via mobile device. The Delta BESS system will be available on market in 2015.
Label
Label
News Source :
Corporate Communications
©
Delta Electronics, Inc. All Rights Reserved.