3/31/2014
Delta Electronics' Innovative Intelligently-controlled
LED Lighting Solutions to Shine at Light+Building 2014
Amsterdam, March 31, 2014 - Delta Electronics, Inc., the leading global provider of power and thermal management solutions, today announces it will unveil a broad spectrum of innovative intelligently-controlled LED lighting solutions with industry-leading quality, reliability and ease of maintenance at Light+Building 2014 in Frankfurt. Delta's leadership in energy conversion efficiency combined with the breakthrough wireless connectivity and auto-dimming features of our LED product portfolio empower the concept of green cities and buildings across the EMEA region by enabling remarkable energy conservation. Delta's value-added proposition includes:
• Outdoor LED Street Lighting Solutions:
Delta's latest street lights SLDQ series boast the unique capability of integrating a wireless control platform within their power supply system, an outstanding breakthrough in the LED lighting industry. A highly efficient performance of ~110 lm/W and a prolonged life cycle guarantee significant energy savings. The lightweight (6.5 Kg) and modular design of our street lights in terms of optics, thermal dissipation and electrical components, enables prime ease of installation, maintenance while facilitating future component upgrades.
• Commercial LED Tubes and Panel Lights:
Delta's LED panel lights are auto-dimmable technology in accordance with the surrounding light intensity through a unique embedded DALI (Digital-addressable Lighting Interface) sensor for detection and control functionalities. Innovative dimmable technology combined with leading efficiency of up to 130 lm/W (and power factor of >0.95) for our AC LED tubes result in considerable energy and opex savings for facilities that strive to attain the green building concept.
• Driver-on-Board (DOB) LED Light Engines:
The advanced DOB technology developed by Delta boasts a slim, light-weight design and operates directly with an AC input, thus, offering a more favorable cost structure to installers by eliminating the need of external AC to DC LED drivers. Their high power factor (>0.95) and anti-electric shocks polymer coating position these products as the leading solutions in the industry in terms of environment-friendliness and safety. They also offer an integrated dimmable circuit compatible with most dimmers available in the market and with no flickering effects.
• Indoor Retrofit LED Bulbs and Spot Lights:
Delta's LED bulbs and spot lights enable significant energy savings through a flexible design that allows for direct replacement of energy-inefficient incandescent, CFL and halogen spot lights. In addition, this product line embeds a state-of-the-art circuit design that offers smooth dimming properties with no flicker and is compatible with most dimmers in the market.
Light+Building 2014 is the world's largest trade fair for lighting and intelligent green buildings. Welcome to visit Delta's stand at Messe Frankurt Hall 4.1 Stand k70.