6/24/2013
Delta Sponsors Ultra Marathon Runner Kevin Lin in the Gobi Desert
Ensures Quality of Video Documentary with Innergie and Qumi Portable Devices
Taipei, Taiwan, June 24, 2013 - Kevin Lin, a renowned Taiwanese ultra marathon runner, set off from Bei'er Lake, Mongolia, for a nearly 40-day, 3,200 kilometer-long extreme adventure run across the perilous Gobi Desert. Despite Mongolia's harsh summer weather in the desert, Lin will periodically upload high-definition videos and photos taken during the journey via satellite to his official website and share his challenges in the tough environment including water scarcity and extreme weather. Lin's efforts aim to raise public awareness of water issues and the importance of environmental protection.
Sponsored by Delta Group, a video documentary of Lin's Gobi adventure will participate in international movie festivals for the purpose of environmental education. To ensure video quality and a sufficient power supply for related devices throughout Lin's journey in the Gobi Desert, Delta has provided its newly launched Innergie PocketCell Duo battery bank and the Vivitek Qumi Q7 HD LED portable projector as secret weapons for the team.
The PocketCell Duo is the world's smallest dual USB 6,800mAh rechargeable battery bank. Approximately the size of two lipstick holders side-by-side, the PocketCell Duo features an impressive power capacity of 6,800mAh, and dual USB power ports that enable users to charge any combination of two tablets or smart phones simultaneously. Combined with a protection suite, the PocketCell Duo can provide Lin with a highly reliable power solution anytime, anywhere. The Qumi Q7 delivers up to 800 lumens and a 30,000:1 contrast ratio with an LED light source. It also features high definition (HD) and high resolution with large widescreen image projection of up to 107-inches that will enable Lin and his team to review daily videos on a large screen in his tent.
Lin will upload videos and photos taken during his Gobi adventure run to his official website to share with the public. You are welcome to follow Lin's Gobi adventure via his website and send your support and encouragement to the whole team!
- KEVINLIN website:http://www.kevinlin.org<2013 Expedition Gobi>
- JOURNAL: http://www.kevinlin.org/KL/KL1-3journal.html
- MEDIA: www.kevinlin.org/KL/KL1-4photo.html
About Innergie PocketCell Duo
PocketCell Duo is the world's smallest dual USB 6,800mAh rechargeable battery bank, bundled with two 2.1Ah fast charging USB power ports and the critically acclaimed Magic Cable Trio, which features a mini-USB tip, a micro-USB tip, and the Apple 30-pin connector. That means that the PocketCell Duo is compatible with the iPhone, iPad, iPod, as well some of today's popular Android and Blackberry smart phones and PCs. An array of LED indicators line the power button which, when plugged into a USB-chargeable device, activates the charging process and provides an indication of its power reserves when unplugged. An array of LEDs indicate the power reserve status or charging status when plugged into a USB charging port. Combined with a protection suite that includes short circuit protection, over temperature protection, over current protection, over power protection and over voltage protection—the PocketCell Duo provides users with a highly reliable power solution for power-users, frequent travelers or more, anytime, anywhere.
About Vivitek Qumi Q7
The Qumi Q7 delivers up to 800 lumens and 30,000:1 contrast ratio with an LED light source that gives it up to 30,000 hours of operation time. It features high definition (HD) and high resolution with a large widescreen image projection up to 107-inches and offers easy portability, weighing only 1.39kg. The Q7 is also 3D-ready via Texas Instruments' DLP®1 Link™ and incorporates 2D-to-3D content conversion technology that takes any existing 2D content and immediately projects it into a 3D visual effect.