9/25/2023

Delta Electronics Foundation and National Museum of Marine Science & Technology Set Up Asia's First Zero-Carbon Coral Conservation Center for Endangered Corals

Delta Electronics Foundation and the National Museum of Marine Science & Technology (NMMST) have jointly announced the opening of the Chaojing Coral Conservation Center on September 23rd  with the aim of restoring internationally recognized endangered corals. By leveraging Delta Electronics' expertise in industrial and building automation, and also integrating intelligent aquaculture and environmental management, the Center intends to create a suitable and energy-efficient greenhouse for coral growth. Corals with heat-resistant genes will be selected and transplanted into the Wanghaixiang Chaojing Bay Resource Conservation Area. It is expected that over 10,000 corals will be restored within three years. In addition, Delta will contribute renewable electricity to help the Chaojing Coral Conservation Center eventually become the first of its kind in Asia to reach zero carbon emissions.

Bruce Cheng, Delta’s founder and Chairman of the Delta Electronics Foundation, said, "Global climate change is intensifying, and research by the United Nations expects that 70% to 90% of coral reefs may face extinction while a quarter of marine species may lose their habitat if planet Earth’s average temperature rises above 1.5°C. Hence, the Delta Foundation launched a coral restoration initiative in 2021. The new Chaojing Coral Conservation Center will bolster our cooperation with the NMMST, with Delta's automation technology supporting key processes within the research of heat-resistant corals. This will help corals in Taiwan and beyond to develop better heat-resistant resilience in the face of more frequent marine heatwaves."

Su-Fen Chen, Director-general of NMMST, remarked, "Over and above being only the first coral conservation base in Taiwan to integrate with a marine protected area, the Chaojing Coral Conservation Center is also an important site for environmental education. The public can make an appointment to visit, with the museum curators and Delta volunteers serving as lecturers, and learn the importance of corals in marine ecology. They can also experience planting coral seedlings to protect marine biodiversity and contribute to a healthy ocean.

Shan Shan Guo, Delta’s Chief Brand Officer and Vice Chairman of the Delta Electronics Foundation, underscored, " Keelung is a beautiful city located at the intersection of mountains and sea. It is also seen by experts as the Noah's Ark for corals, as they migrate northward due to the warming of the surrounding waters of Taiwan. The Delta Foundation is honored to collaborate with coral experts from the NMMST. In addition to assisting in the establishment of the center and using in Delta's automated breeding equipment, we are also working together on research projects with experts, and joining hands with conservation organizations to promote and expand marine education. We would like to express our gratitude to the many experts who have guided Delta along the way. We hope that Delta's efforts will encourage more people in Taiwan to value the restoration of coral habitats, and together, become caretakers of coral.”

The Chaojing Coral Conservation Center is located next to the Keelung Wanghaixiang Chaojing Bay Resource Conservation Area and was built with over USD 1 million funded by the Delta Electronics Foundation. Integrating high-efficiency coral farming systems and intelligent building automation systems, the area can support the cultivation of about 6,000 coral seedlings. Currently, the center has selected 20 endangered native coral species in Taiwan are listed on the International Union for Conservation of Nature (IUCN) Endangered and Vulnerable Coral List, including Turbinaria reniformis, Galaxea astreata and Pavona cactus, which have been identified among the first protected species in the center. And through molecular biological identification, those corals are confirmed as local species, using Delta's Micro Computed Tomography (Micro CT) to produce 1μm high-resolution images and establish a database of Calcium carbonate skeletons of endangered corals. The Delta Foundation also continues to collaborate with NMMST and conservation organizations on educational programs. This allows more people to participate in coral restoration courses offered by the center, gaining a nearby understanding of the importance of coral ecosystems to Taiwan's marine ecology. This early adaptation helps mitigate the impacts of global warming on Taiwan's ecosystem.

News Source:Delta electronics