06/16/2026Delta Accelerates Equipment Development and Validation for ZEISS Taiwan with SECS / GEM Solution DIASECS
As advanced packaging drives semiconductor manufacturing toward multi-station collaboration, equipment must exchange increasing volumes of process, status, and production data. To ensure seamless connectivity with factory control systems, manufacturers must comply with SECS / GEM standards. However, communication requirements often vary across semiconductor fabs, including differences in data formats, functional specifications, and integration approaches. Combined with fragmented development tools and inconsistent system architectures, these challenges increase customization efforts and development complexity, as well as prolong project timelines. As a result, the industry is seeking communication solutions that combine standardized frameworks with flexible configuration. In the semiconductor ecosystem, ZEISS is a leading provider of optical metrology, inspection, and defect analysis solutions for wafer fabrication and advanced packaging. To enhance equipment connectivity and system integration, ZEISS Taiwan has aimed to establish a SECS / GEM-compliant communication framework. However, varying customer requirements and collaboration across teams in Taiwan, Singapore, and Germany have increased project complexity, highlighting the need of a communication solution that supports standardization, flexibility, and rapid deployment. To address these challenges, Delta’s DIASECS Semiconductor Equipment Communication and Control Software and expert consulting are helping ZEISS Taiwan swiftly develop and validate equipment communication to meet global fab integration standards. Delta has simplified complex factory specifications into intuitive functions. Through sample code, multilingual technical support, and comprehensive training, Delta has enabled engineering teams to quickly master communication workflows, API implementation, and system logic, overcoming the hurdles of limited experience and cross-border collaboration. Designed with flexible configurations, the DIASECS supports diverse equipment types across various industries, including semiconductors, PCBs, solar energy, and electronic components. By adopting the DIASECS-GEM Library, ConfigTool, and FASimulator, ZEISS Taiwan successfully verified communication logic early in the design stage. This reduced reliance on physical machine testing and significantly shortened the overall development cycle. Delta’s DIASECS Semiconductor Equipment Communication and Control Software offers the following benefits ● Standardized Equipment Communication x High-Speed Data Exchange: DIASECS provides a SECS / GEM-compliant communication framework that enables equipment standardized communication functions while reducing repetitive development and customization efforts. Its standardized architecture also simplifies system integration, future expansion, and maintenance. Supporting up to 300 transactions per second, it meets the high-frequency, high-volume communication demands of advanced packaging production lines. ● User-Friendly Development Tools for Faster Implementation: The DIASECS-GEM Library supports GEM (E30) and GEM300 standards, transforming complex communication logic into easy-to-use APIs that reduce the need for in-depth SECS-II expertise. Combined with ConfigTool’s intuitive graphical interface and built-in validation mechanisms, it simplifies configuration, minimizes setup errors, and lowers the learning curve for more efficient implementation. ● Simulation-Based Validation for Rapid Development: FASimulator simulates communication between host systems and equipment, supporting early functional validation and stress testing before physical equipment is available. This reduces reliance on on-site testing and accelerates development. ● Comprehensive Traceability for Efficient Maintenance: Raw data and SML communication logs provide full traceability of message exchanges between equipment and host systems, enabling faster issue diagnosis, more efficient troubleshooting, and shorter development and deployment cycles With Delta’s DIASECS Semiconductor Equipment Communication and Control Software, ZEISS Taiwan has streamlined equipment communication development and integration. The solution accelerated deployment to global semiconductor fabs while enhancing equipment interoperability and smart manufacturing efficiency, delivering benefits across the semiconductor value chain.