09/11/2020AIoT Video Surveillance Upgrades Medical Environmental Security Protection
According to the Deloitte 2017 Global Healthcare sector outlook report, healthcare spending is projected to reach $8.7 trillion globally in 2020. In Taiwan from 2019 to 2020, according to the Taiwanese Ministry of the Interior, the national average life expectancy rose nine weeks to 80.7 years. Moreover, according to statistics provided by the National Health Insurance Administration (NHI), the average person made 15 medical visits per year in Taiwan. In addition to schools and offices, hospitals have thus become the places we access frequently in our daily life. The prime issue developing out of this trend toward longevity is how we can secure the safety of both patients and medical professionals while also enhancing the business intelligence of hospitals. The Internet of Medical Things (IoMT) is an amalgamation of medical devices and applications that can connect to health care information technology systems using networking technologies. According to Frost & Sullivan, the IoMT is expected to grow at a Compound Annual Growth Rate (CAGR) of 26.2% to reach $72 billion by 2021. The IoMT already plays a vital role in transforming the healthcare industry and will clearly continue to do so. Going beyond traditional surveillance, in the era of IoT IP surveillance systems have implemented Artificial Intelligence (AI) and been transformed by powerful edge-computing devices. Such AI-driven solutions can reduce the load on manual management while also mitigating the risk of both employee and customer infection under COVID-19.There is also an increasing number of hospitals that have adopted IP surveillance and business intelligence systems, allowing business owners to transform real-time images into big-data analysis. VIVOTEK, the leading global IP surveillance solution provider, introduces 6 IP surveillance solutions dedicated to specific locations within a hospital: 1.Emergency entrance: Acting as the frontline of hospitals, the difference between life and death is a split-second decision taken by doctors in the emergency room. The ability to discern details even in video taken under high-contrast lighting conditions is extremely important for security applications such as the entrance of emergency room. In this scenario, VIVOTEK recommends the adoption of IP surveillance systems with Wide Dynamic Range (WDR) technology. VIVOTEK has developed a comprehensive range of WDR implementations to suit customer needs. WDR Pro represents advancement over WDR Enhanced, utilizing a hardware-based solution that simultaneously captures two or three images at different exposure levels. An algorithm is then used to combine the images into a single frame of video in which all areas are optimally exposed for maximum visibility. WDR Pro II is a further improvement, capturing four images simultaneously for even more enhanced clarity of video. It can optimize image quality in challenging lighting environments and offers crystal clear video images of emergency room entrances throughout the day and night. 2.Lobby and nursing station: Hospital Lobbies provide complex functionality including cashiers, customer service, and pharmacies that are often crowded. In this multi-functional venue, VIVOTEK recommends the use of 360-degree panoramic fisheye IP surveillance network cameras. These advanced devices offer surround views with zero blind spots, meaning they can provide total coverage of wide, open areas. VIVOTEK is a leader in the field of those specializing in fisheye cameras, and its 360-degree panoramic fisheye cameras are equipped with its self-developed Smart VCA (Video Content Analysis). With human-centered AI based deep-learning technology, this feature can enhance operational efficiency by offering higher accuracy and fewer false alarms. Further, in the era of smart healthcare, VIVOTEK's video management software VAST 2 can integrate with Health Information systems (HIS) to combine medical records, prescriptions, and payment sheets with video footage. Operators can set up keywords to receive event notification through the triggering of a relevant alarm. 3.Corridors: An increasing number of hospitals are expanding into roles as local health centers, and thus also expanding their functionality with multiple buildings. Each building in such complexes is usually connected via a long corridor. Even in the out-patient area, the space is commonly designed with corridor access to a waiting area. It is for this reason that VIVOTEK's cameras are equipped with Corridor Mode, enabling video rotation that better captures the perspective of narrow corridors, hallways or aisles and maximizes image visibility without sacrificing peripheral monitor space. 4.Datacenter, laboratory and VIP room: In the critical areas such as data centers, laboratories and VIP rooms, IoMT can enhance protection and service through AI-driven Video Content Analysis. VIVOTEK adopts an advanced AI engine for people detection and has developed Smart VCA technology that provides higher accuracy and fewer false alarms. The on-board VIVOTEK Smart VCA suite includes advanced detection of Intrusion, Loitering, Line-Crossing, Unattended Objects, Missing Objects, Faces, and Crowds. Moreover, VIVOTEK has integrated CyberLink's FaceMe® AI facial recognition engine into its IP surveillance solutions. Through this strengthened alliance, facial recognition intelligence will be integrated with VIVOTEK's network cameras and back-end video management software, enabling security operators to receive accurate facial recognition alerts based on both blacklists and whitelists. 5.Elevator: Hospital elevators are an ideal location for the implementation of mini type IP surveillance systems. VIVOTEK's ultra-mini fixed dome network camera is designed with a tiny diameter of only 90 mm that is smaller than your palm, and is armed with Rugged IK10 design housing, capable of withstanding the impact of a 5 kg mass dropped from 400 mm above the impacted surface. With tamper detection, the camera is capable of detecting incidents such as redirection, blocking or defocusing, or even spray paint. Due to its compact and intelligent design, it offers security but remains discrete. 6.Parking areas: VIVOTEK introduces its License Plate Recognition (LPR) camera, featuring built-in License Plate Recognition software and all-in-one edge-computing capability without the need for additional servers. The camera also offers efficient access control management through black & white lists and centralized maintenance of multi-site cameras, meaning that security staff of parking areas with multiple entry points no longer need to upgrade systems one at a time. They can simply upload these lists to a single centralized LPR camera and all the other LPR cameras will download the master list, significantly reducing both installation time and maintenance effort. Learn more about all-in-one LPR. During the COVID-19 pandemic, thermal imaging scanners help to prevent the spread of the disease by detecting individuals with elevated body temperature in areas of high foot traffic. VIVOTEK offers a Crowd Control Solution for businesses to maintain maximum occupancy as well as a safer and healthier environment. Its 3D stereo counting camera designed with dual lens provides precise tracking and a counting accuracy up to 98%, making it ideally suited for hospital entrances, operation rooms and restricted areas. AIoT has transformed network and information technology in Smart Healthcare, but its rapid rise has made it a target for cyber-attacks. There is also an increasing number of cyber-attacks involving healthcare extortion and stolen medical records. Medical professionals are able to access databases and medical records in a very short time, however, such highly connected devices and data increase the need for cybersecurity. Highly attune to such developments, VIVOTEK's network cameras and video recorders are embedded with Trend Micro's anti-intrusion software with multi-layer protection allowing security managers to respond faster to threats and minimize cyber-risks in smart healthcare.