Q: Delta DIAVision DMV-VGR: How do I perform shape matching for object recognition?

1. Open the project in the DMV-VGR software and click “Flow Edit.”



2. Add "Shape" from the toolbox to the flow, and then click “Save.”



3. After returning to the project page, the shape matching function will appear with an exclamation mark

(indicating that parameters have not been set).




4. Click "Shape" to enter the detailed settings page, and then define the ROI and the object area.



5. Click “Save” to display the recognition results along with the object shape.


Keywords: Vision, DMV-VGR, Object Recognition, Shape Matching