How do I set up the Modbus TCP Client on the Industrial Robot DRV/DRS?


 
1. Use software to connect to the robot arm.
2. Click .
3. Navigate to the tab.
4. In the communication settings section, set to .
5. Click to write the communication settings.
6. Click to confirm that the communication settings are correct.