How can I check the status of a TCP/IP connection for VTScada and solve the connection error issues?
           
          
          
              You can check the status value on the TCP/IP connection tab under the Tag page. The value 0 means there is no error and the connection is normal.  For any other value, you can use the F1 shortcut key and enter "TCP/IP Port Tags" to look up the meaning of the error code.