How do I import customized plug-in functions into the Machine Vision Platform DIAVision?
           
          
          
              1. Creating Plug-Ins: Follow the instructions in 
Chapter 5 Plug-In Development of the 
DIAVision Operation Manual to create plug-ins. You may also contact Delta's sales representatives or authorized distributors for help. The following image shows plug-in examples.
 
2. DIAVision sets the default path for plug-ins as 
C:\Users\Public\Documents\DMV-IVS\Plugin. Create a new folder with the name 
KludgeCircleFitting. You may save your plug-ins here.
 
3. Launch 
DIAVision > 
Help > 
Plugin Information. Check if the plug-ins are imported successfully.
 
4. Click “
+” to add new components, and then double click on 
KludgeCircleFitting. The plug-in is now imported into the detection process and can be used.