For Delta’s CNC Solution NC5 Series’ MPG, why is the status of the DI signals X32-X39 contrary to that of the MLC software?
           
          
          
              The DI polarities can be adjusted by parameter settings. By default, the MPG’s DI polarity is set as “0” (Normal close). The X32~X39 signals are changed to positive direction when the parameters N5.2.0~N5.2.7 are set as “1” (as below).