To use the arm controller, which specific wiring connections must be completed first?
Before using the arm controller, connections must be fully completed, including those for safety, system digital I/O signals, the teach pendant, and the arm. Only after these connections are properly wired can the controller function normally. Please refer to the wiring diagram below for guidance.