How do I conduct motor homing using DIADesigner-AX?
Please set up motor homing by following the steps below.
1. Select the motor that requires homing in the “Devices” window (see Image 1) on the left-hand side of the DIADesigner-AX interface.
Image 1
2. Click “Homing Setting” on the left, and select “Homing Mode.” Then, set “Homing speed during search for switch,” “Homing speed during search for z phase pulse,” and “Homing Acceleration” (see Image 2).
Image 2
3. Execute MC_Home. Fill in the name of the motor that requires homing at “Axis”, and the position value of the origin at “Position” (see Image 3).
Image 3
4. Trigger “Execute,” and when “Done” shows “True,” the motor homing is complete (see Image 4).
Image 4