How do I install EDS files on the PC-Based Motion Controller AX-8 Series?
Click "Tools" on the menu bar, and click "Device Repository..." (See Image 1) → Click "Install" (See Image 2) → Select the EDS file to be installed → Click “Open”

Image 1

Image 2