How do I set the pulse parameters of servo drives?
Step 1: Run ASDA-Soft and select the Parameter Editor. Input 0x0000 for the parameter P1-01, and press “Enter” to cycle the power.
Step 2: Change the P1-00 external pulse input type setting and select the pulse type.