How do I set Inverter_MS300 to output analog signal (AFM)?
Please refer to the following steps.
Step 1: Connect to MS300 via VFD Explorer Lite as follows.
Step 2: After making the connection, click on PR→click on Load Pr. to read the parameters.
Step 3: Open parameter table 03 group, and select 03-20 AFM output signal.
Step 4: Set 03-31 AFM analog output signal.
Step 5: After confirming the DIP switch and wiring method, you can use the analog output of the inverter.