How do I reset the IP address of the HMI DOP-100 Series?

Step 1: Long press the upper-left corner until it displays five icons.


Step 2: Click the first “gear” Icon > A System Info pop-up appears > Click “YES”.


Step 3: Select the “System Setting”.


Step 4: Click the tab on the lower-right corner to enter the next page.


Step 5: Click the “Network” tab > Reset the IP address.