How do I check the logic of I/O terminal signals in the Delta Vector Control Drive C2000 Series?
The I/O terminal signals refer to the digital input and output signals. The logic of the input signals can be observed from the parameter 02-50. The output signal logic can be learned with the parameter 02-51.
Image 1
Image 2