Can Delta’s CNC controller convert DXF files to G-Code?
Yes. Please press the button EDITon the CNC controller and then the button PRG. Select the DXF function on the controller screen, and select a desired DXF file. Enter parameters to the pop-up setting screen, and select Convert to convert from the file to G-code.