How do I select an operating mode for the cooling fan of the C2000?
Users can select an operating mode for the cooling fan of the C2000 by setting the parameters 07 ~ 19 according to the current ambient temperature.

Parameters for setting up cooling fans of different frames are listed below.