2.Open the “EIP Builder”.
3.Drag the device icon onto the network diagram or use auto-scanning to upload the device onto the network diagram through a network connection.
4.Open “Data Mapping”.
5.Set the communication address and download it to the PLC.
6.Set up the AC motor drive’s EIP communication card: IP address, frequency, operation source and set Pr.09-30 to 0.