The manual prohibits all tilting to prevent damage during transportation. The packaging of the AP2000 wooden box is not designed for lifting from the side, and tilting the wooden box may damage the APF2000 inside (see the figure below). Once the APF2000 is removed from the box, tilting at an angle is allowed for only short-term purposes such as passing through a narrow door.